Dual Display 24Paral and MIPI DSI on IMX7Dual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual Display 24Paral and MIPI DSI on IMX7Dual

812 Views
dmitriychertov
Contributor I

Hi everyone.

I have a question: can I connect two indicators to IMX7Dual on the 24-bit parallel interface and on the MIPI DSI and simultaneously display a different picture or video? There are separate controllers for each interface or there is one controller for two interfaces?

In Reference Manual I find only this info in 13.4.3.9.2 chapter: "MIPI DSI Master supports dual display". But I want to use both interfaces.
I see many questions about dual displays, but not on the IMX7Dual with these two interfaces.

Labels (2)
Tags (2)
0 Kudos
Reply
2 Replies

650 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Dmitriy,

    There is only one LCDIF in i.MX7D, So it can't support dual display! For your solution, you had better use i.MX6DL.


Have a great day,
TIC weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

650 Views
alex001
Contributor I

I have the same question to ask

0 Kudos
Reply