Dual 1080p video playback in sabresd-imx6d

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual 1080p video playback in sabresd-imx6d

798 Views
chandrasekharma
Contributor III

Hi all,

Help me to configure VPU properly to play two 1080p@30fps videos in Freescale sabresd-imx6 dual core. As per attached document Page No. 28 Dual 1080p@30 (TBD)

Query: Whether this feature support in Freescale sabresd-imx6 board?

If yes then help me to share configuration information for reference

Thanks in advance

0 Kudos
1 Reply

487 Views
igorpadykov
NXP Employee
NXP Employee

Hi chandrasekhar

it is supported with VPU >300MHz, please check examples on

https://community.freescale.com/docs/DOC-93449

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos