Dts file corresponding to imx single, dual, dual lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dts file corresponding to imx single, dual, dual lite

2,955 Views
dilshad_alam
Senior Contributor II

Imx6 SoC has variants, Single , Dual, Dual lite.

Could some one tell respective .dts files for these variants.

I can see the relevant one only is

imx6q-sabresd.dts

Labels (1)
0 Kudos
Reply
8 Replies

2,465 Views
dilshad_alam
Senior Contributor II

I know above things. I guess I have not put forward my question straight.

imx6dl.dtsi

imx6dl-sabreauto.dts

imx6dl-sabreauto-ecspi.dts

imx6dl-sabreauto-flexcan1.dts

imx6dl-sabreauto-gpmi-weim.dts

imx6dl-sabresd.dts

imx6dl-sabresd-hdcp.dts

imx6dl-sabresd-ldo.dts

imx6dl-wandboard.dts

imx6q-arm2.dts

imx6q-arm2-hsic.dts

imx6qdl.dtsi

imx6qdl-sabreauto.dtsi

imx6qdl-sabresd.dtsi

imx6q.dtsi

imx6q-sabreauto.dts

imx6q-sabreauto-ecspi.dts

imx6q-sabreauto-flexcan1.dts

imx6q-sabreauto-gpmi-weim.dts

imx6q-sabrelite.dts

imx6q-sabresd.dts

imx6q-sabresd-hdcp.dts

imx6q-sabresd-ldo.dts

imx6q-sbc6x.dts

imx6sl.dtsi

imx6sl-evk-csi.dts

imx6sl-evk.dts

imx6sl-evk-ldo.dts

Lets take SabreSD Board.. Which DTS file we should refer for Single, Dual, Dual Lite and Quad models.

0 Kudos
Reply

2,465 Views
BiyongSUN
NXP Employee
NXP Employee

q for Q and Dual

dl for Dual Lite and Solo

sl for  Solo Lite

0 Kudos
Reply

2,465 Views
dilshad_alam
Senior Contributor II

Would be much helpful if you can tell single dts file for ex:-

imx6dl-sabresd.dts :-  I belive its for SabreSD dual Lite models

Like Solo lite I am seeing this

imx6sl-evk-csi.dts

imx6sl-evk.dts

imx6sl-evk-ldo.dts

which one is correct?

0 Kudos
Reply

2,465 Views
BiyongSUN
NXP Employee
NXP Employee

dual lite and solo share the same but with different core number.

imx6sl-evk-csi.dts      with csi and ldo bypass version

imx6sl-evk.dts            without csi and ldo bypass version

imx6sl-evk-ldo.dts      without csi and ldo enable version

0 Kudos
Reply

2,465 Views
dhavalvadhar
Contributor IV

Hi Biyong,

I think CSI stands for 'Camera Serial Interface'. But what does LDO stand for?

Thanks,

Dhaval

0 Kudos
Reply

2,465 Views
BiyongSUN
NXP Employee
NXP Employee

CMOS Sensor Interface (CSI)

It is for using the internal PMU LDO or not.

Please check the datasheet.

IMX6SLCEC.pdf

Untitled.png

Untitled.png

0 Kudos
Reply

2,465 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

2,464 Views
BiyongSUN
NXP Employee
NXP Employee

cd kernel_imx/arch/arm/boot/dts

ls |grep dts|grep mx6

0 Kudos
Reply