Driver for the PMIC MC34VR500V3ES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Driver for the PMIC MC34VR500V3ES

818 Views
satish_k_singh
Contributor III

Hello ,

Could you please let know where can i find the driver for the PMIC MC34VR500V3ES or any reference driver for the PMIC.

0 Kudos
Reply
1 Reply

764 Views
Pavel
NXP Employee
NXP Employee

The NXP KITVR5100FRDMPGM board provides an ideal platform for programming the VR5100 OTP. See the AN5403 Application Note:

https://www.nxp.com/docs/en/application-note/AN5403.pdf

 

NXP SDK for i.mx contains drivers for PMIC using. See attached file.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply