when I Download the images(IMX6Q) into the MMC on Ubuntu12.04,
I used cmd :$ sudo dd if=u-boot.imx of= /dev/sdx bs=1K seek=1; syncbut I can not find /dev/sdx.
I have found mmc\SD card can not be loaded under Ubuntu12.04 system, But I can use the MFGTOOS in Windows to download the firmware to the board
May I ask what is the reason? How can i solve it?
How can i solve it?
try lsblk or df to find your /dev/sdx
you can use sd card reader, insert card to the reader, then use sudo fdisk -l, the pc will list your sd card, sdb or sdc,
then use dd if=
Thanks a lot! But I used command “sudo fdisk -l” I can not find sdb or sdc!
Please tell me what to do next,
ps:I can download firmware on Windows successfully with MfgTool
sdx means sd partition you use, like sdb, for more detailed informatio, you can refer to the chapter 4.3.1 Preparing the card of imx linux user guide.
Thanks Joan, which document about imx linux user guide?please tell me this file name or download links,
thanks a lot!
pls focus on the chapter 4.3.1 Preparing the card and chapter 4.3.2 Copying the full SD card image
thank you very much