Download the images into the MMC on Ubuntu12.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Download the images into the MMC on Ubuntu12.04

3,458 Views
jerrylee008
Contributor II

when I Download the images(IMX6Q) into the MMC on Ubuntu12.04,

I used cmd :$ sudo dd if=u-boot.imx of= /dev/sdx bs=1K seek=1; sync
but I can not find /dev/sdx.

I have found mmc\SD card can not be loaded under Ubuntu12.04 system,
But I can use the MFGTOOS in Windows to download the firmware to the board
May I ask what is the reason
How can i solve it?

Labels (1)
0 Kudos
Reply
7 Replies

3,314 Views
floriankoenig
Contributor II

try lsblk or df to find your /dev/sdx

0 Kudos
Reply

3,314 Views
tian
Contributor I

you can use sd card reader, insert card to the reader,   then use  sudo fdisk -l,  the pc will  list your sd card, sdb or sdc,

then use   dd if=

0 Kudos
Reply

3,314 Views
jerrylee008
Contributor II

Thanks  a lot! But I used command “sudo fdisk -l”   I can not find sdb or sdc!

Please tell me what to do next,

ps:I can download firmware on Windows successfully with MfgTool

0 Kudos
Reply

3,314 Views
joanxie
NXP TechSupport
NXP TechSupport

sdx means sd partition you use, like sdb,  for more detailed informatio, you can refer to the chapter 4.3.1 Preparing the card of imx linux user guide.

0 Kudos
Reply

3,314 Views
jerrylee008
Contributor II

Thanks Joan, which document about imx linux user guide?please tell me this file name or download links,

thanks a lot!

0 Kudos
Reply

3,311 Views
joanxie
NXP TechSupport
NXP TechSupport

pls focus on the chapter 4.3.1 Preparing the card and chapter 4.3.2 Copying the full SD card image

0 Kudos
Reply

3,311 Views
jerrylee008
Contributor II

thank you very much

0 Kudos
Reply