Download onnxruntime-imx.git.tar.gz of SDK 5.15.71 to report errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Download onnxruntime-imx.git.tar.gz of SDK 5.15.71 to report errors

1,021 次查看
pengluo
Contributor III

When downloading and compiling SDK 5.15.71, I executed the bitbake imx-image-full command and found that the onnxruntime 1.10.0 r0 do_ Fetch always fails. After reading the log, it was found that the package onnxruntime imx. git. tar. gz failed to download. I followed the link and found that the package did not exist. Please help confirm whether the path of this software package has changed and update the. bb file. Thank you!

 

The error message is as follows:

DEBUG: Mirror fetch failure for url https://mirrors.kernel.org/yocto-sources/git2_github.com.nxp-imx.onnxruntime-imx.git.tar.gz (original url: gitsm://github.com/nxp-imx/onnxruntime-imx.git;protocol=https;branch=lf-5.15.71_2.2.0;name=runtime)
DEBUG: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1464"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/sysroots-uninative/x86_64-linux/usr/bin:/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/work/armv8a-poky-linux/onnxruntime/1.10.0-r0/recipe-sysroot-native/usr/bin/python3-native:/work/imx-yocto-bsp-5.15.71/sources/poky/scripts:/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/work/armv8a-poky-linux/onnxruntime/1.10.0-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/work/armv8a-poky-linux/onnxruntime/1.10.0-r0/recipe-sysroot/usr/bin/crossscripts:/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/work/armv8a-poky-linux/onnxruntime/1.10.0-r0/recipe-sysroot-native/usr/sbin:/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/work/armv8a-poky-linux/onnxruntime/1.10.0-r0/recipe-sysroot-native/usr/bin:/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/work/armv8a-poky-linux/onnxruntime/1.10.0-r0/recipe-sysroot-native/sbin:/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/work/armv8a-poky-linux/onnxruntime/1.10.0-r0/recipe-sysroot-native/bin:/work/imx-yocto-bsp-5.15.71/sources/poky/bitbake/bin:/work/imx-yocto-bsp-5.15.71/build-xwayland/tmp/hosttools"; export HOME="/home/mx"; /usr/bin/env wget -t 2 -T 30 --passive-ftp -P /work/imx-yocto-bsp-5.15.71/downloads/ 'https://mirrors.kernel.org/yocto-sources/git2_github.com.nxp-imx.onnxruntime-imx.git.tar.gz' --progress=dot -v failed with exit code 8, no output

0 项奖励
回复
3 回复数

1,004 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 项奖励
回复

893 次查看
DRAVE
Contributor III

Hi, @Zhiming_Liu 

How to solve this problem?  Which file do you want to change?

 
0 项奖励
回复

441 次查看
kylin_wan
Contributor I

I also want to know how it solve!

0 项奖励
回复