Download line

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Download line

640 次查看
Mohan51
Contributor II

Where can i find the  download line in imx93 evk.then i can use that line and flash the latest os.

I set the boot mode to CORTEX-M(then i am able to detect the usb in usb1 port), because i am unable to detect the usb if it is in CORTEX-A mode.

 

I am flashing the latest BSP LINUX6.6.0_1.0.0 for imx93 evk.

 

While flashing the image using uuu.I am getting this error.

"""LF_v6.6.3-1.0.0_images_IMX93EVK$ sudo uuu uuu.auto-imx93-11x11-lpddr4x-evk
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Success 0 Failure 1


3:1 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -f imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot"""

0 项奖励
回复
1 回复

608 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Here you met unable to detect the usb if it is in CORTEX-A mode, you can try to setting the SW1301“0100” from low to high when in the download mode. If it still not work tell me.

0 项奖励
回复