Dot matrix printer printing issue in IMX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dot matrix printer printing issue in IMX6ULL

Jump to solution
1,167 Views
Prial_03
Contributor III

I am using imx6ull in which i interface TVS MSP 270 Classic Plus USB Dot Matrix Printer with following pkgs in yocto project:
cups, cups-filters, ghostscript, and build image, in it service is successfully started without any error, printer is also added with lpadmin command and destination is also set without any errors the problem is lp command executed successfully without any error but printer is not printing. 

I checked the hardware connections everything is perfect, i tried with canon laser printer same issue persist in that also.

I tested same commands in Ubuntu PC and it worked

Labels (4)
0 Kudos
Reply
1 Solution
1,145 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Make sure that you have enable the port where the printer is connected, also make sure that this is in the kernel configuration file.

Regards

View solution in original post

0 Kudos
Reply
1 Reply
1,146 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Make sure that you have enable the port where the printer is connected, also make sure that this is in the kernel configuration file.

Regards

0 Kudos
Reply