Dot matrix printer printing issue in IMX6ULL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dot matrix printer printing issue in IMX6ULL

ソリューションへジャンプ
1,164件の閲覧回数
Prial_03
Contributor III

I am using imx6ull in which i interface TVS MSP 270 Classic Plus USB Dot Matrix Printer with following pkgs in yocto project:
cups, cups-filters, ghostscript, and build image, in it service is successfully started without any error, printer is also added with lpadmin command and destination is also set without any errors the problem is lp command executed successfully without any error but printer is not printing. 

I checked the hardware connections everything is perfect, i tried with canon laser printer same issue persist in that also.

I tested same commands in Ubuntu PC and it worked

ラベル(4)
0 件の賞賛
返信
1 解決策
1,142件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Make sure that you have enable the port where the printer is connected, also make sure that this is in the kernel configuration file.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,143件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Make sure that you have enable the port where the printer is connected, also make sure that this is in the kernel configuration file.

Regards

0 件の賞賛
返信