Dose anyone confirm the function of HDMI output at XGA mode using android_jb4[1].2.2_1.1.0-ga ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dose anyone confirm the function of HDMI output at XGA mode using android_jb4[1].2.2_1.1.0-ga ?

1,966 Views
takaya
Contributor I

Hi,

Does anyone confirm the functionality of HDMI output at XGA mode using android_jb4[1].2.2_1.1.0-ga and iMX6D SEBRE ?

If you have recommended configurations, setup or resolution commands, please let me know.

takaya

Labels (1)
0 Kudos
Reply
5 Replies

1,781 Views
igorpadykov
NXP Employee
NXP Employee

Hi takaya

strictly speaking XGA mode 1024×768 is not listed in

supported modes in Table 33-3 "Video Modes"  IMX6DQRM

i.MX 6Dual/6Quad Applications Processor Reference Manual.

Seems operation depends on particular monitor, because some monitors work

well with i.MX6 at XGA.

First you should use true HDMI monitor and check if it supports XGA:

try this from Linux command line:

cat /sys/class/graphics/fb0/modes

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,781 Views
takaya
Contributor I

Thank you for your prompt reply.

According to the Manual you introduced, XGA 1024x768 is not listed in the table 33-3.

I'm still looking into the section in details, but I'd like to ask.

?? Does HDMI Tx block have the capability to transfer image date at XGA mode ??

?? Can we see proper pictures at XGA mode with some modification of BSP and iMX configuration ??

If anyone has such experience, I'd like to share the information.

I really appreciate your assistance.

regards,

takaya

0 Kudos
Reply

1,781 Views
igorpadykov
NXP Employee
NXP Employee

Hi takaya

 

Operation depends on particular monitor, because some monitors work

well with i.MX6 at XGA.

First you should use true HDMI monitor and check if it supports XGA:

try this from Linux command line:

cat /sys/class/graphics/fb0/modes

Best regards

chip

0 Kudos
Reply

1,781 Views
takaya
Contributor I

Executed modes command for fb0, fb1 and fb2.

root@android:/ # cat /sys/class/graphics/fb0/modes

D:1024x768p-60

root@android:/ # cat /sys/class/graphics/fb1/modes

U:240x320p-60

root@android:/ # cat /sys/class/graphics/fb2/modes

S:640x480p-60

S:720x576p-50

S:720x480p-60

S:720x480p-60

S:1280x720p-50

S:1280x720p-60

S:1920x1080p-50

S:1920x1080p-60

V:640x480p-60

V:1280x1024p-60

V:1024x768p-60

V:640x480p-60

root@android:/ # cat /sys/class/graphics/fb2/mode

V:1024x768p-60

root@android:/ #

How's the result ?

What's suitable configuration for XGA mode ?

regards,

takaya

0 Kudos
Reply

1,781 Views
igorpadykov
NXP Employee
NXP Employee

Hi takaya

 

Operation depends on particular monitor

and not guaranteed.

Best regards

chip

0 Kudos
Reply