Hi,
Regarding i.MX Plus EVK(evk_8mp) Ethernet ENET2(J8)
The attached file (patch file) is for #2_Ethernet Port on IMX8MP EVK. for Android 11.0.0_2.4.0, ethernet ENET2(ENET2:J8)..
This patch file is working well based on Android 11.0.0_2.4.0.
Then, Its patch file is not working based on the android 12.0.0_1.0.0 for #2 Ether port please ** i.MX 8MPlus EVK(evk_8mp) Ethernet ENET2(J8)
What is the problem?
** Original Android BSP for IMX8MP is not working for ENET2(ENET2:J8) on the IMX8MP EVK
解決済! 解決策の投稿を見る。
I give update in the case you create, please check it, so close it here.
Wish you have a nice day
I give update in the case you create, please check it, so close it here.
Wish you have a nice day
Hi, I also use android 12.0.0_1.0.0 for dual ethernet port, please send me the update file, thanks!
Hi, I also use android 12.0.0_1.0.0 for dual ethernet port, please send me the update file, thanks!
Hi,
Thank you so much.
Could you reshare the file as I can no longer download it?
BR
Domenico Acri
I email to you just now, please check it.
Hi, I use android 12.0.0_2.0.0 for dual ethernet port, please send me the update file, thanks!
@JungWonLee I already email to you, please have a check.
Wish you have a nice day
Hi Rita_Wang,
do you happen to have an EthernetDual package for Android 12?
Or even the apk?
BR
Domenico Acri
Hi,
thank you very much.
You could also send me the patches:
0001-android-vendor-fsl_imx_demo-dual-ethernet-demo.patch
.....
to include the project?
BR
Domenico Acri
Hi,
thank a lot for the answer.
But is the package compatible with Android 12?
When I apply the patch "0001-android-vendor-fsl_imx_demo-dual-ethernet-demo.patch",
I have the Android.bp.rej file and some files that the patch should delete are not present.
Best Regards
Domenico Acri