Doing DMA on imx6Q with linux.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Doing DMA on imx6Q with linux.

1,387 Views
amanmehta
Contributor I

Hi,

I am using imx6Q and want to perform DMA transfers m2m , being quite new to the driver side, I was looking forward if you could point me to example code/ Manual for writing the code.

Thanks 

Labels (2)
0 Kudos
Reply
1 Reply

1,117 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aman

one can look at unit test sdma example

module_test - imx-test - i.MX Driver Test Application Software 

Measure SDMA Memory To Memory Copy Performance on i.MX6Q 

Freescale i.MX SDMA tutorial (part I) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply