As described on wayland web site that xwayland has backward compatibility to allow X cliend to run.
And I have seen that there is "xwayland" in i.max8m yocto project.Here are the commands I used:
The question is can X client, or for example LXDE or XFCE, runs on this image?
For the i.MX boards that have a GPU, the imxgpu-viv recipes package the graphic components for each DISTRO – X11, frame buffer (FB), XWayland,Wayland backend, and Weston compositor. The xwayland is support in our BSP. But
For X client, or for LXDE or XFCE you need to realize yourself.
may i take it that xwayland support xfce?but when i run startxfce4,then error.
what is the reason for this?please help me slove this problem.thanks!