Does x11 and gstreamer compete on display ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does x11 and gstreamer compete on display ?

1,593 Views
rans
Senior Contributor I

Hello,

I use yocto morti with x11 distro, and try to display gstreamer on screen.

qt5 application shows without any issue.

But gstreamer pipelines are distorted with green lines. I use rtp pipeline. simpler pipeline with videotstsrc, looks better.

I suspect that x11 is competeing on same display. On stopping the gstreamer application, the desktop manager pops in. even if I try to display x11 with :

systemctl set-default multi-user.target

I still get xterm terminal pop in.

We also noticed high memory bus usage, even before starting pipeline (read is about 450MB/s in mddc profiler)

So, it makes us suspect that they compete on the display.

1. Is it that x11 yocto distro should not be used with gstreamer, and we better change to fb distro ?

2. Can I disable x11 completely ?

3. Is it possible to command gstreamer pipeline to display on the other hdmi output (there are 2 hdmi outputs in board) ?

Regards,

Ran

0 Kudos
Reply
4 Replies

1,204 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ran

please try nxp offical bsps and nxp gstreamer plugins described on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

for x11 please refer to attached Linux Manual Chapter 17 X Windows Acceleration

for disabling x11 check Yocto Guide sect.5.1 Build configurations.

Gstreamer examples are given in sect.7 Multimedia Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,204 Views
rans
Senior Contributor I

Hi Igor,

I created fb distro, but even with fb distro, I still get xterm in hdmi output !

Is there a way to get rid of it ?

Regards,

Ran

0 Kudos
Reply

1,204 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ran

what processor used in the case, please try with Demo Images from

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor

0 Kudos
Reply

1,204 Views
rans
Senior Contributor I

Hello Igor

We are still struglling with this issue...

Now we suspect that it is a matter of ethernet paket loss.

I have opened a new question here:

https://community.nxp.com/thread/466146 

Regards

Ran

0 Kudos
Reply