Does the i.MX6 Solo Light support SDIO Simplified Specification Part E1, Version 3.00.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the i.MX6 Solo Light support SDIO Simplified Specification Part E1, Version 3.00.

2,045 Views
aworthi
Contributor II

It’s a little confusing since the SDIO is an extension of the SD Spec.  The way I read it, v3.0 could effectively be supported.  The Datasheet states SDIO Card specification, Part E1, v1.10, it explicitly states UHS-I SDR104 mode at 104 MB/s which was introduced in SDIO Card specification, Part E1, v3.00.  So it looks like it can handle the speed.  Are there any other features introduced in v2.00 or v3.00 that are not supported?

Thanks in advance

Tags (2)
0 Kudos
Reply
4 Replies

1,777 Views
igorpadykov
NXP Employee
NXP Employee

Hi aworthi

datasheet IMX6SLCEC p.14 states

IMX6SLCEC  rev.3  4_2014  p.14.jpg

one can find differencies between 1.10 and 3.0 versions on links below

Latest Simplified Specifications - SD Association

Archive - SD Association

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,777 Views
aworthi
Contributor II

Igor,

I understand this from the specifications.  But it seems that the SDIO also supports UHS-I SDR104 mode (104 MB/s max) which is specified in version 3.0.  Are there any other features greater than 1.10 that are implemented?  If I want to run SDIO at 104 MB/s are there any limitations?

Thank you. 

0 Kudos
Reply

1,777 Views
Yuri
NXP Employee
NXP Employee

  Really there are some terminology inaccuracies with SD / MMC specs in our documentation.
As for MMC - 104 MB/s max can be acnieved under 8-bit transfer mode up to 52 MHz in DDR mode.

For SD - maximum frequency is 50 MHz, bus width = 4 bit.

~Yuri.

0 Kudos
Reply

1,777 Views
igorpadykov
NXP Employee
NXP Employee

Hi aworthi

I do not think that smth implemented above mentioned in documentation,

there are no limitations with SDR104.

Best regards

igor

0 Kudos
Reply