Hi all,
Does the i.MX28 Windows CE 6.0 BSP support having the registry hive on the SD card? I noticed a question regarding this on another i.MX device and a response from Adeneo was that it was not supported for SD, just for NAND.
I was wondering if the i.MX28 BSP will allow the use of an SD registry? If so has anyone implemented this and could give me some pointers?
I have read the Microsoft documentation but was wondering if there is anything specific in the BSP I should watch out for.
Kind regards, Mark
Deactivated user are you available to help on this case?
Adeneo Engineering Team can you confirm if you are available to help on this case?