Does the beta release of Lollipop support booting from NFS/TFTP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the beta release of Lollipop support booting from NFS/TFTP?

3,029件の閲覧回数
huanxinjiang
Contributor I

We are developing an instrument based on the i.MX 6 and have worked with the alpha and beta releases of Android Lollipop on the Sabre-SD board. The issue is, we want to boot the board through TFTP/NFS but don't know how to, there is also not enough information on the UserGuide of the releases. Can you give me the guidance for booting from NFS/TFTP?

More detailed information:

1. It is okay to load a kernel image through u-boot/TFTP to the memory (0x10008000) of the Sabre-SD board.

2. The uImage is used (compiled with "make uImage LOADADDR=0x10008000), per the user guide of the beta release.

3. I noticed it is necessary for 4.4.3 to set device tree information, should we do this too? But how to specify the addresses?

Here is the u-boot log. It stopped after printing the line "Starting kernel ..."

FEC Waiting for PHY auto negotiation to complete.. done

BOOTP broadcast 1

BOOTP broadcast 2

DHCP client bound to address 129.196.210.225

Using FEC device

TFTP from server 129.196.211.60; our IP address is 129.196.210.225

Filename 'uImage'.

Load address: 0x10008000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##########

         1.8 MiB/s

done

Bytes transferred = 6814664 (67fbc8 hex)

## Booting kernel from Legacy Image at 10008000 ...

   Image Name:   Linux-3.10.53-88177-g589371c

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    6814600 Bytes = 6.5 MiB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

   XIP Kernel Image ... OK

No gpc device node -9, force to ldo-enable.

Starting kernel ...

ラベル(2)
タグ(3)
0 件の賞賛
返信
6 返答(返信)

2,360件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Huanxin,

Now that Lollipop is released are you able to boot through TFTP?

0 件の賞賛
返信

2,360件の閲覧回数
huanxinjiang
Contributor I

Hi Sergio,

Yes the GA release supports boot through TFTP but I followed the kk.4.4.3 doc (there is no doc about this on 5.0's user guide). It works for me although I rarely use it due to other reasons.

thanks,

Huanxin

0 件の賞賛
返信

2,360件の閲覧回数
fdu
Contributor II

Nice to know that it works over NFS.

But I tried it with no success.

When executing "class_start main",  eth0 stop so it died...

Is it possible to have your patchs in init.rc & init.freescale.rc to support NFS

Best regards.

0 件の賞賛
返信

2,360件の閲覧回数
alandeng123
Contributor III

HI All,

I am using:

Android™ User's Guide, Rev. L5.0.0_1.0.0-ga, 06/2015

In the doc, there is not info about how to do NFS boot.

I managed this following kk4.3.3 doc.

and can download img and start kernel.

However, there is a problem after started the kernel.

see the bold lines, after that, it seems board cannot have an IP anymore.

Something is wrong in the image.

in Ubuntu, I ping the board all the time, after the the kernel started, I can still ping the brd.

however, after thie msg:

                 nf_conntrack: automatic helper assignment is deprecated and it will be removed soon. Use the iptables CT target to attach helpers instead.

Ubuntu ping has no resp anymore.

Something is wrong in the image.

Compare this with KK4.4.3 NFS, I can ping board all the time after kernel started.

Anyone can help on this?

Alan

===============================================

ALSA device list:

  #0: wm8962-audio

  #1: imx-hdmi-soc

VFS: Mounted root (nfs filesystem) on device 0:13.

devtmpfs: mounted

Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)

init: /dev/hw_random not found

Console: switching to colour dummy device 80x30

init: /dev/hw_random not found

rfkill: BT RF going to : off

init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'

binder: 147:147 transaction failed 29189, size 0-0

init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'

init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

ñread descriptors

read strings

mtp_bind_config

android_work: sent uevent USB_STATE=CONNECTED

android_work: sent uevent USB_STATE=DISCONNECTED

android_work: sent uevent USB_STATE=CONNECTED

android_usb gadget: high-speed config #1: android

android_work: sent uevent USB_STATE=CONFIGURED

healthd: BatteryTemperaturePath not found

healthd: BatteryTechnologyPath not found

root@sabresd_6dq:/ # nf_conntrack: automatic helper assignment is deprecated and it will be removed soon. Use the iptables CT target to attach helpers instead.

root@sabresd_6dq:/ # nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

0 件の賞賛
返信

2,360件の閲覧回数
alandeng123
Contributor III

I added this

androidboot.selinux=disabled androidboot.dm_verity=disabled

in bootarg to get my result.

ow, it died early.

0 件の賞賛
返信

2,360件の閲覧回数
alandeng123
Contributor III

Sometimes, nf_conntrack: automatic helper assignment is deprecated and it will be removed soon. Use the iptables CT target to attach helpers instead.

does not comes out.

However, ping lost resp around the bold part.

Alan

===============

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

android_usb: already disabled

read descriptors

read strings

mtp_bind_config

android_work: sent uevent USB_STATE=CONNECTED

android_work: sent uevent USB_STATE=DISCONNECTED

android_work: sent uevent USB_STATE=CONNECTED

android_usb gadget: high-speed config #1: android

android_work: sent uevent USB_STATE=CONFIGURED

binder: 147:147 transaction failed 29189, size 0-0

root@sabresd_6dq:/ # healthd: BatteryTemperaturePath not found

healthd: BatteryTechnologyPath not found

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

nfs: server 10.68.1.88 not responding, still trying

0 件の賞賛
返信