Does the MFGtool requires the Serial Downloader Boot mode over IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the MFGtool requires the Serial Downloader Boot mode over IMX6

1,456 Views
adityanagal
Contributor III

HI , 

I am working over IMX6 solo based target board . I learnt that , boot device can be programmed using MFGtool . My question is , to program using the MFGtool , does the boot configuration settings for the IMX6 solo need to be set to the Serial Downloader mode. Please conform. 

Regards, 

Aditya Nagal

0 Kudos
Reply
1 Reply

1,068 Views
joanxie
NXP TechSupport
NXP TechSupport

for how to set board , you can refer to the linux user guide, which depends what device you use, mmc, sd card or nand flash, for more detailed information, pls refer to the chapter 4.5 How to boot the i.MX boards of enclosed file.

0 Kudos
Reply