Does the IMX8MQ chip with kernel 5.10.72 support dual screen display?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the IMX8MQ chip with kernel 5.10.72 support dual screen display?

132 Views
ximenbingmeng
Contributor III

We are trying to upgrade the kernel of the IMX8MQ chip to a higher version, but we would like to confirm whether kernel 5.10.72 supports dual screen display, and what should be the effect of dual screen display?
a. The guessing effect, if the fbset command is input, should both resolutions be displayed? So how do I check the refresh rate of two screens?
b. Alternatively, if the mipi screen is a desktop system and the HDMI screen is fb0, can this be considered as achieving a different display?
c.Can Weston achieve dual framebuffer display?
d.How to open debugging information for DRM?

0 Kudos
Reply
1 Reply

102 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, its supported,

A1. Yes, you have to checked the two screen, also you have to change the uboot setting the default don't support dual screen.

A2. Yes

A3.Yes,

A4. the GPU is binary you can't debug it.

For better performance you need upgrade your kernel version.

Regards

0 Kudos
Reply