Does the Ethernet Controller on the i.MX 6Solo uses DMA?.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the Ethernet Controller on the i.MX 6Solo uses DMA?.

Jump to solution
1,522 Views
andresgonzalez
Contributor II

Hi Freescale Community.

We are using the Ethernet Controller of i.MX 6Solo processor and we are not sure if this controller uses DMA in any way.

Could somebody please clarify me if DMA is used by this controller and the purpose of its usage?.

Thanks in advance.

P.D.: We are using the Legacy Buffer Descriptors.

Labels (3)
1 Solution
1,410 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andres

yes i.MX6S ENET module has own DMA engine - "uDMA", one

can find its references in particular in

IMX6SDLRM sect. 23.5.14.1 Enhanced receive buffer descriptor:

"This section discusses the enhanced uDMA receive buffer descriptor..."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
1,411 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andres

yes i.MX6S ENET module has own DMA engine - "uDMA", one

can find its references in particular in

IMX6SDLRM sect. 23.5.14.1 Enhanced receive buffer descriptor:

"This section discusses the enhanced uDMA receive buffer descriptor..."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,410 Views
andresgonzalez
Contributor II

Thanks for your help.

0 Kudos
Reply