Does scfw of i.max8qm support three or four container for boot img

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does scfw of i.max8qm support three or four container for boot img

1,674 Views
zbm030823
Contributor II

Hi everyone,

   As you see,  there are two containers referenced which are primary and second container  for boot by SCFW of I.max8qm.If we modify the boot img supporting three containers,does  scfw of i.max8qm support three or four container for boot img?

0 Kudos
Reply
4 Replies

1,530 Views
zbm030823
Contributor II

Hi igorpadykov,

     It seems that you don't answer exactly about my question.I want the answer about i.max8qm which includes 4 A53 and 2 A72,but i.maxqx which only includes 4 A35 from you.After all,thanks for your reply.How to support three containers for boot img of i.max8qm is still a big probrem interrupting me.

0 Kudos
Reply

1,530 Views
igorpadykov
NXP Employee
NXP Employee

answer for i.MX8QM is the same as for i.MX8QXP.

Please note that since i.MX8QM is not officially released yet, there

is no support for it. Support for not publicly released (PRE-PRODUCTION)

processors is provided through nxp local marketing office.

Best regards
igor

0 Kudos
Reply

1,530 Views
zbm030823
Contributor II

Hi igor,

Thanks.

0 Kudos
Reply

1,530 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhu

there are Image Container Set0 and Set1 on Figure 5-1. Layout of Boot Device
and as described in sect.5.9 Boot image i.MX8DQXP Reference Manual :

Every Container Set includes two containers. One container (SECO container) for SECO
FW , and another container (SCU container) for SCU FW (necessary), AP IPL (optional),
CM4 FW (optional), and DDR initialization image (optional).

https://www.nxp.com/docs/en/reference-manual/IMX8DQXPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply