Does mx25 requires SwapBBI support in NAND driver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does mx25 requires SwapBBI support in NAND driver?

Jump to solution
738 Views
rohith1z
Contributor III

Hi,

I'm running a custom kernel on a custom board based on mx25.

It has a 2GB micron nand flash.(2k+64B spare)

Kernel is based freescale L2.6.28 release.

I became aware of  the SwapBBI issue/feature with the NFC(attached document), when investigating nand corruption issues.

The newer releases have a swap BBI feature in the mxc nand driver.

My query is: Is this applicable to MX25 so that I can back port the driver?

Obviously I would need to propagate the changes to boot loader and factory flash programmer.

In some forums, I read that it would be applicable to only imx31 and imx27 and hence the confusion.

Labels (3)
0 Kudos
1 Solution
520 Views
shaojun_wang
NXP Employee
NXP Employee

Yes, you can back port the swap bbi driver from newer bsp to older bsp, include kernel, uboot and factory flash programmer.

View solution in original post

0 Kudos
1 Reply
521 Views
shaojun_wang
NXP Employee
NXP Employee

Yes, you can back port the swap bbi driver from newer bsp to older bsp, include kernel, uboot and factory flash programmer.

0 Kudos