Does mx25 requires SwapBBI support in NAND driver?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does mx25 requires SwapBBI support in NAND driver?

ソリューションへジャンプ
929件の閲覧回数
rohith1z
Contributor III

Hi,

I'm running a custom kernel on a custom board based on mx25.

It has a 2GB micron nand flash.(2k+64B spare)

Kernel is based freescale L2.6.28 release.

I became aware of  the SwapBBI issue/feature with the NFC(attached document), when investigating nand corruption issues.

The newer releases have a swap BBI feature in the mxc nand driver.

My query is: Is this applicable to MX25 so that I can back port the driver?

Obviously I would need to propagate the changes to boot loader and factory flash programmer.

In some forums, I read that it would be applicable to only imx31 and imx27 and hence the confusion.

ラベル(3)
0 件の賞賛
1 解決策
711件の閲覧回数
shaojun_wang
NXP Employee
NXP Employee

Yes, you can back port the swap bbi driver from newer bsp to older bsp, include kernel, uboot and factory flash programmer.

元の投稿で解決策を見る

0 件の賞賛
1 返信
712件の閲覧回数
shaojun_wang
NXP Employee
NXP Employee

Yes, you can back port the swap bbi driver from newer bsp to older bsp, include kernel, uboot and factory flash programmer.

0 件の賞賛