Does miracast function have relationship with LCD resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does miracast function have relationship with LCD resolution

ソリューションへジャンプ
2,708件の閲覧回数
xiaoqianlin
NXP Employee
NXP Employee

Hi,

One customer used MX6DL with 480X800 LCD RGB interface(JB4.2.2) and reported  error  when connecting two devices using miracast, I attached the log, can you help to check?

Regards,

Linda

Linda Lin
0 件の賞賛
返信
1 解決策
2,532件の閲覧回数
Ivan_liu
NXP Employee
NXP Employee

Hi Linda,

Does the customer use the wifi display sink apk developed by themselves.

The display size doesn't impact the miracast function.

BRs,

Ivan

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,533件の閲覧回数
Ivan_liu
NXP Employee
NXP Employee

Hi Linda,

Does the customer use the wifi display sink apk developed by themselves.

The display size doesn't impact the miracast function.

BRs,

Ivan

0 件の賞賛
返信
2,532件の閲覧回数
xiaoqianlin
NXP Employee
NXP Employee

Thanks. Checked with customer, they downloaded the source code and compile it.

Linda Lin
0 件の賞賛
返信
2,532件の閲覧回数
YixingKong
Senior Contributor IV

Ivan.liu, could you hep the customer's issue?

Thanks,

Yixing

0 件の賞賛
返信