Does mimxrt1064 support external flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does mimxrt1064 support external flash

1,650件の閲覧回数
StarMao159376
Contributor II

Does the MCU rt1064 support booting from external SPI flash? Or does it only support booting from internal flash?

0 件の賞賛
返信
3 返答(返信)

1,632件の閲覧回数
bennxp
Contributor III

So clarify, the 1064 has the FlexSPI2 wired to internal flash, so it cannot be used to boot from external flash. Depending on your needs, you can write a program to the internal flash that will simply execute code from the external flash, which will look a lot like booting from external flash.

0 件の賞賛
返信

1,638件の閲覧回数
StarMao159376
Contributor II

Thanks

0 件の賞賛
返信

1,643件の閲覧回数
b36401
NXP Employee
NXP Employee

i.MXRT1064 supports FlexSPI2, SD and eMMS boot devices.