Does mimxrt1064 support external flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does mimxrt1064 support external flash

848 次查看
StarMao159376
Contributor II

Does the MCU rt1064 support booting from external SPI flash? Or does it only support booting from internal flash?

0 项奖励
3 回复数

830 次查看
bennxp
Contributor III

So clarify, the 1064 has the FlexSPI2 wired to internal flash, so it cannot be used to boot from external flash. Depending on your needs, you can write a program to the internal flash that will simply execute code from the external flash, which will look a lot like booting from external flash.

0 项奖励

836 次查看
StarMao159376
Contributor II

Thanks

0 项奖励

841 次查看
b36401
NXP Employee
NXP Employee

i.MXRT1064 supports FlexSPI2, SD and eMMS boot devices.