Does imx8mq evk load and run program with uboot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does imx8mq evk load and run program with uboot?

1,500 Views
1541189572
Contributor III

I use tftpboot command to load binary program, then run go ${loadaddr} command which physical address is 0x40480000. But a fault occured: 

## Starting application at 0x40480000

"Synchronous Abort" handler , esr 0x02000000

.....

.....

I have tested two bin program. One is imx4_m4_demos/imx8mq_m4_TCM_hello_world.bin and the other is image-imx8_all.bin. They both caused the same problem.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,333 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version of BSP are you using? About the NFS 4.7.5 Running the Linux image from NFS in the i.MX_Linux_User's_Guide document.

And this https://community.nxp.com/docs/DOC-103717  could do help for you.

0 Kudos
Reply

1,333 Views
1541189572
Contributor III

i should use booti ${loadaddr} - ${fdt_addr} when run linux image.

0 Kudos
Reply