Does imx6ul linux use OCRAM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does imx6ul linux use OCRAM?

1,195 Views
charlieschultz
Contributor II

The imx6ul RM says it uses some OCRAM during boot, but after that it is free. Does imx6ul linux use OCRAM? In looking at pm-imx6.c, it is not clear to me with respect to the ul version of the imx6.

Labels (2)
0 Kudos
Reply
1 Reply

1,030 Views
igorpadykov
NXP Employee
NXP Employee

Hi Charlie

yes uses (seems one can use linker map for that), for example

low power driver, described in attached Linux Manual Chapter 21
Low-level Power Management (PM) Driver.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply