We are using iMXRT for one of our products. We need to have httpserver support in that. We tried to run the example httpserver project that came along with sdk (though hidden from the UI). Is there any support to make it work.
Hi Fayiz,
The sdk doesn't guarantee the working of the lwip example codes. Refer this thread for details EVK-MIMXRT1050 SDK middleware projects not available .
Now, to make the project work you have to include the FSL_FEATURE_PHYKSZ8081_USE_RMII50M_MODE definition. This is needed to enable some functions in the phy drivers.
Hi,
SDK 2.4.0 released in May 2018 is addressing these issues.
PetrL