Does iMX28 EVK support latest Linux kernel 3.10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does iMX28 EVK support latest Linux kernel 3.10

1,170件の閲覧回数
santhoshkarthik
Contributor III

Hi,

  In iMX28 EVK software portal they are providing kernel version 2.6. but we are using latest linux kernel version, So Can we use latest Linux kernel 3.10 in iMX28 EVK??

  Can we use Yocto build for Linux kernel 3.10 with iMX28 EVK instead of LTIB.

4 返答(返信)

734件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at the following app note :

"Building for i.MX Mature Boards"

http://www.nxp.com/docs/en/application-note/AN12024.pdf 

Regards,

Yuri.

734件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

mx28 is well supported in mainline kernel, so I suggest you to use the latest one from kernel.org instead of 3.10.

734件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Karthikeyan,

There are BSPs for i.MX processors developed by NXP and there are also BSPs created by a community external to NXP.

You can find the NXP BSPs releases here: git.freescale.com > fsl-arm-yocto-bsp.git

Unfortunately as you said there is no support with Yocto for imx28, however on the other hand the BSP releases developed by the external community can be found here: https://github.com/Freescale

Here you will find Yocto support for imx28, just please note that NXP provides support of the BSPs developed by NXP, but unfortunately the releases of the external community are out of our scope.

If you need support on any of the community's releases you may subscribe the FSL Community BSP mailing list at freescale.github.io to talk directly with the developers and other users.
https://lists.yoctoproject.org/listinfo/meta-freescale

I hope this helps.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

734件の閲覧回数
santhoshkarthik
Contributor III

Hi,

  Can anybody please support on this

0 件の賞賛