Does i.mx 8M plus support UART ISO7816 mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.mx 8M plus support UART ISO7816 mode?

718 Views
AlanYL
Contributor I

Does i.MX 8M Plus support UART IOS7816 mode? Or should I have another microcontroller that integrated ISO UART modules?

Labels (1)
0 Kudos
Reply
1 Reply

704 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The Universal Asynchronous Receiver/Transmitter (UART) provides serial
communication capability with external devices through a level converter and an RS-232
cable or through use of external circuitry that converts infrared signals to electrical
signals (for reception) or transforms electrical signals to signals that drive an infrared
LED (for transmission) to provide low speed IrDA compatibility.
UART supports NRZ encoding format , RS485 compatible 9 bit data format and IrDAcompatible
infrared slow data rate (SIR) format.

You can refer to our reference design:

UART-USB DESIGN.PNG

0 Kudos
Reply