Does i.mx 8M plus support UART ISO7816 mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.mx 8M plus support UART ISO7816 mode?

769件の閲覧回数
AlanYL
Contributor I

Does i.MX 8M Plus support UART IOS7816 mode? Or should I have another microcontroller that integrated ISO UART modules?

ラベル(1)
0 件の賞賛
返信
1 返信

755件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The Universal Asynchronous Receiver/Transmitter (UART) provides serial
communication capability with external devices through a level converter and an RS-232
cable or through use of external circuitry that converts infrared signals to electrical
signals (for reception) or transforms electrical signals to signals that drive an infrared
LED (for transmission) to provide low speed IrDA compatibility.
UART supports NRZ encoding format , RS485 compatible 9 bit data format and IrDAcompatible
infrared slow data rate (SIR) format.

You can refer to our reference design:

UART-USB DESIGN.PNG

0 件の賞賛
返信