Does i.MX8M Mini support 1080p 2D 90degree rotation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX8M Mini support 1080p 2D 90degree rotation?

869 Views
jimmyli
Contributor IV

Hi,

    I have found that the IPU in i.MX6 just can support max. 1024*1024 rotation.

    Now, we need to rotate the max.1080p (or at least 1280*720) 2D picture in 90 degree.

    Does i.MX8M Mini can implement?

    Thanks.

Labels (1)
0 Kudos
4 Replies

573 Views
art
NXP Employee
NXP Employee

Yes, the GC328 2D graphics core of the i.MX8MMini processor supprts the 1920x1080 frame rotation in hardware.


Have a great day,
Artur

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

573 Views
john_weber
Contributor II

Artur,

Do you know if the GC238 has a Gstreamer plugin that works to perform the rotation?

Thanks,

John

0 Kudos

573 Views
art
NXP Employee
NXP Employee

Not absolutely sure, but try it as described in the Section 7.3.16 of the attached document.

Artur

0 Kudos

573 Views
jimmyli
Contributor IV

Hi Artur,

     Thanks for your reply.

0 Kudos