Does i.MX8 can support 60fps camera output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX8 can support 60fps camera output

746件の閲覧回数
xu_ji1
Contributor V

Hi,

Does i.MX8QM can support 60fps camera output or not?

1280X800 @60fps could  i.MX8QM CSI MIPI have capability can receive this camera data all correctly?

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

647件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Xu

yes it can support 60fps, it necessary to use latest version of silicon.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信