Hi, Everybody
I see the spec that iMX6's hdmi support 4k x 2k video format. But I can not see it in 33-3 table.
My question is whether iMX6's hdmi support 3840x2160@30hz resolution(the fps can be less than 30)?
Thank you in advance for your answer.
Regards,
Chao
Solved! Go to Solution.
HI Chao
unfortunately not as IPU max. supported screen size: up to 4096 x 2048 pixels,
HDMI is connected to IPU as shown on p.15,17 presentation
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Chao
unfortunately not as IPU max. supported screen size: up to 4096 x 2048 pixels,
HDMI is connected to IPU as shown on p.15,17 presentation
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
I tried to create a screen of 4096x2048 with fbset on wandboard with iMx6DualLite :
- fbset -g 4096 2048 4096 2160 32 -t 4500 4 4 4 4 12 4
I have some error with DI0 counter because the DIO counter have only 12 bits resolution (DI0 Sync Wave Gen 2 Register 0).
imx-ipuv3 2400000.ipu: DI0 for 1 counters out of range.
imx-ipuv3 2400000.ipu: DI0 for 2 counters out of range.
So how i can create a screen of 4096x2048 resolution.
Thanks
Julien
Bnd if I don't use IPU to draw the picture, should it support the 4k x 2k resolution?
Thank you!
Thank you for your kindly reply! But I am curious about that why some background of the resolution is green and some about white and blue in p 15 of the Document? I can not see any explain in that document... Do you know what does it mean?
Thank you!