Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

925 Views
m_c
Senior Contributor I

Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

Labels (2)
0 Kudos
Reply
1 Reply

727 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

IPU CSI supported resolutions do not depend on sync mode and

CSI BT.656 can be supported with these resolutions too.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply