Does i.MX6 MMDC or DDR cal tool support read leveling?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6 MMDC or DDR cal tool support read leveling?

Jump to solution
844 Views
torus1000
Contributor V

Hi,

I heard QorIQ Configuration Suite (QCS) support read adjust method
(read leveling) as following.

Automatic CAS to preamble calibration:

Instead of JEDEC’s MPR method, Freescale controllers use a

proprietary method of read adjust method. Auto CPO will provide the

expected arrival time of preamble for each strobe line of each byte

lane during the read cycle to adjust for the delays cased by the fly-by

topology

Does DDR calibration tool for i.MX6* also support this feature?

* such as:
     i.MX6/7 DDR Stress Test Tool V2.20
     https://community.freescale.com/docs/DOC-105652
     i.MX6 DDR Stress Test Tool V1.0.3
     https://community.freescale.com/docs/DOC-96412

Thanks.

Labels (1)
0 Kudos
1 Solution
652 Views
Yuri
NXP Employee
NXP Employee

Hello,

  As I understand the question relates to DQS gating feature, described

in section 12 (DQS Gating ) of app note AN4467 (i.MX 6 Series DDR Calibration).
The DDR Stress Test Tool performs DQS gating calibration.

i.MX6/7 DDR Stress Test Tool V2.30


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
653 Views
Yuri
NXP Employee
NXP Employee

Hello,

  As I understand the question relates to DQS gating feature, described

in section 12 (DQS Gating ) of app note AN4467 (i.MX 6 Series DDR Calibration).
The DDR Stress Test Tool performs DQS gating calibration.

i.MX6/7 DDR Stress Test Tool V2.30


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
652 Views
torus1000
Contributor V

I see. Thank you for your correct answer.

I read User Guide then found a description as following:

The read DQS gating calibration is used to adjust the read DQS gating with the middle of the

read DQS preamble.

It seems as same as  QCS without using MR3[2:0] ={MPR,MPR loc}.

0 Kudos