Hi
We have a customized camera which would send multiple data types within a frame on each virtual channel. We are studying for a product which can support this input. In i.MX6DP/QP's reference manual, it needs to set one data type to each CSI unit (such as CSI0_MIPI_DI3/CSI0_MIPI_DI2/CSI0_MIPI_DI1/CSI0_MIPI_DI0). Does this means CSI0 in IPU1, for example, can only receive one data type in a frame?
Thank you.
Hi Igor,
Sorry, I don't get how can I stored all the data with different types into the memory if only one data type can be received by a CSI module in the IPU at a time.
Could you please give me more instructions?
Thank you very much.
Kethy
Hi Kethy
>Does this means CSI0 in IPU1, for example, can only receive one data type in a frame?
yes this is correct, in general frame with different types can be stored in memory then parsed in software.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------