Hi community,
We have a question about i.MX6DQ Linux BSP.
We want to confirm whether i.MX6DQ Linux BSP support Wi-Fi access point mode.
We guess the AR6003 driver for SABRE bord can work as access point mode, but don't know whether there is software to evaluate the mode.
Would you let me know the status of each Linux BSP?
(e.g. L3.0.35_4.1.0: NO, L3.10.17_1.0.0-ga & L3.10.35_1.0.0-ga: YES)
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Hi Satoshi Shimoda,
Please refer to "i.MX_6Dual6Quad_Linux_Reference_Manual.pdf" in "L3.0.35_4.1.0_130816_docs" which can be downloaded from FSL official web, its "Chapter 40 AR6003 WiFi " introduce it is a standard linux wifi device.
Wifi module of AR6003 works normally we tried before in i.MX6Q-SDP. You can use comand " iwconfig " to set it work mode(iwconfig --help can get help).
"iwconfig wlan0 mode master" to setup AP mode after your Wlan up.
refer to:
http://blog.csdn.net/goodlixueyong/article/details/6461871
iwconfig工具使用-windowsbbs126-ChinaUnix博客
Have a nice day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi Shimoda,
Please refer to "i.MX_6Dual6Quad_Linux_Reference_Manual.pdf" in "L3.0.35_4.1.0_130816_docs" which can be downloaded from FSL official web, its "Chapter 40 AR6003 WiFi " introduce it is a standard linux wifi device.
Wifi module of AR6003 works normally we tried before in i.MX6Q-SDP. You can use comand " iwconfig " to set it work mode(iwconfig --help can get help).
"iwconfig wlan0 mode master" to setup AP mode after your Wlan up.
refer to:
http://blog.csdn.net/goodlixueyong/article/details/6461871
iwconfig工具使用-windowsbbs126-ChinaUnix博客
Have a nice day
Best Regards
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Please someone help me.
If AR6003 driver in Linus BSP does not support access point mode, we have to consider modifying the code or changing the Wi-Fi chip.
Best Regards,
Satoshi Shimoda
Hi Satoshi Shimoda,
About the access point mode can be supported in linux I am not sure, Let me confirm it for you. I will give you reply when I get the result.
Have a nice day
Best Regards
Dan