Does i.MX6 Linux BSP provide software to evaluate AR6003 access point?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX6 Linux BSP provide software to evaluate AR6003 access point?

ソリューションへジャンプ
2,050件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

We have a question about i.MX6DQ Linux BSP.

We want to confirm whether i.MX6DQ Linux BSP support Wi-Fi access point mode.

We guess the AR6003 driver for SABRE bord can work as access point mode, but don't know whether there is software to evaluate the mode.

Would you let me know the status of each Linux BSP?

(e.g. L3.0.35_4.1.0: NO, L3.10.17_1.0.0-ga & L3.10.35_1.0.0-ga: YES)

Best Regards,

Satoshi Shimoda

ラベル(6)
タグ(1)
0 件の賞賛
返信
1 解決策
1,761件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi Shimoda,

Please refer to "i.MX_6Dual6Quad_Linux_Reference_Manual.pdf" in "L3.0.35_4.1.0_130816_docs" which can be downloaded from FSL official web, its  "Chapter 40 AR6003 WiFi "  introduce it is a  standard linux wifi device.

    Wifi module of AR6003  works normally we tried before  in  i.MX6Q-SDP. You can use  comand " iwconfig " to set it work mode(iwconfig  --help can get help).

"iwconfig wlan0 mode master" to setup AP mode after your Wlan up.

refer to:

http://blog.csdn.net/goodlixueyong/article/details/6461871

iwconfig工具使用-windowsbbs126-ChinaUnix博客

Have a nice day

Best Regards

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,762件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi Shimoda,

Please refer to "i.MX_6Dual6Quad_Linux_Reference_Manual.pdf" in "L3.0.35_4.1.0_130816_docs" which can be downloaded from FSL official web, its  "Chapter 40 AR6003 WiFi "  introduce it is a  standard linux wifi device.

    Wifi module of AR6003  works normally we tried before  in  i.MX6Q-SDP. You can use  comand " iwconfig " to set it work mode(iwconfig  --help can get help).

"iwconfig wlan0 mode master" to setup AP mode after your Wlan up.

refer to:

http://blog.csdn.net/goodlixueyong/article/details/6461871

iwconfig工具使用-windowsbbs126-ChinaUnix博客

Have a nice day

Best Regards

Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,761件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Dan Wang,

Thank you for your reply.

OK, I understood it supports Wi-Fi AP mode and how to setup the mode.

I appreciate your detail explanation.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,761件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi Shimoda,

It's my pleasure and I am very glad it can help you.

Have a nice day.

Best Regards

Dan

0 件の賞賛
返信
1,761件の閲覧回数
satoshishimoda
Senior Contributor I

Please someone help me.

If AR6003 driver in Linus BSP does not support access point mode, we have to consider modifying the code or changing the Wi-Fi chip.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,761件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Satoshi Shimoda,

About the access point mode can be supported in linux I am not sure, Let me confirm it for you. I will give you reply when I get the result.

Have a nice day

Best Regards

Dan

0 件の賞賛
返信
1,761件の閲覧回数
satoshishimoda
Senior Contributor I

Would you be able to help?

0 件の賞賛
返信