Does i.MX6/7 DDR stress test tool check all DDR addresses?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX6/7 DDR stress test tool check all DDR addresses?

Jump to solution
1,249 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a simple question about i.MX6/7 DDR stress test tool.

(i.MX6/7 DDR Stress Test Tool V2.40 )

Would you let me know whether the tool checks all DDR addresses or check a part of it?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
1 Solution
722 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The Stress tool uses board script (Load Init Script), which provide

memory initialization. All memory, which size is defined via the script (row, col, etc),

is tested.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
723 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The Stress tool uses board script (Load Init Script), which provide

memory initialization. All memory, which size is defined via the script (row, col, etc),

is tested.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply