Does i.MX6/7 DDR stress test tool check all DDR addresses?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does i.MX6/7 DDR stress test tool check all DDR addresses?

跳至解决方案
1,313 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a simple question about i.MX6/7 DDR stress test tool.

(i.MX6/7 DDR Stress Test Tool V2.40 )

Would you let me know whether the tool checks all DDR addresses or check a part of it?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1 解答
786 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The Stress tool uses board script (Load Init Script), which provide

memory initialization. All memory, which size is defined via the script (row, col, etc),

is tested.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
787 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The Stress tool uses board script (Load Init Script), which provide

memory initialization. All memory, which size is defined via the script (row, col, etc),

is tested.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复