Does i.MX 6 Quad can support two CSI-2 MIPI interface cameras working simultaneously?
The i.MX6 supports single MIPI CSI-2 channel, since it may be connected to CSI IPU
via the single gasket. Please look at Figure 19-1 (CSI2IPU gasket connectivity) of the
i.MX6 (DQ) Reference Manual.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Yuri
thank you for your reply.
you mean that i can't connect two MIPI CSI-2 cameras to i.mx6?
here we want to develop an automotive binocular vision system to capture two cameras simultaneously and then image processing to get stereoscopic vision.
could i use two parallel cameras?
Hello,
please refer to app note AN5305 (MIPI–CSI2 Peripheral on i.MX6 MPUs).
http://www.nxp.com/assets/documents/data/en/application-notes/AN5305.pdf
Also, please look at
https://community.nxp.com/message/868547?commentID=868547#comment-868547
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------