Does g2d support G2D_RGB888 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does g2d support G2D_RGB888 ?

2,737 次查看
brenhale
Contributor I

The G2D API format enumeration describes G2D_RGB888 as a 24-bit RGB option (enum #10).

However attempts to use this, even for very simple blit operation yield errors for either invalid src or dst format.

g2d_blit_2d: Invalid src format 10!

There is no errata for lack of support for this. Should it work?

Tested on imx8mm.

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

2,617 次查看
michaelnazzaren
Contributor I

Hi

I have the same problem. Can we have a folowup? Android 10 is my bsp base on

int ret;
void* g2dHandle = getHandle();
struct g2d_buf s_buf, d_buf;
struct g2d_surface s_surface, d_surface;

s_buf.buf_paddr = tmpBuf.mPhyAddr;
s_buf.buf_vaddr = tmpBuf.mVirtAddr;
d_buf.buf_paddr = dstBuf.mPhyAddr;
d_buf.buf_vaddr = dstBuf.mVirtAddr;

s_surface.format = G2D_RGB888;
s_surface.planes[0] = (long)s_buf.buf_paddr;
s_surface.left = 0;
s_surface.top = 0;
s_surface.right = src->width();
s_surface.bottom = src->height();
s_surface.stride = src->width();
s_surface.width = src->width();
s_surface.height = src->height();
s_surface.rot = G2D_ROTATION_0;

d_surface.format = (g2d_format)convertPixelFormatToG2DFormat(dst->format());
d_surface.planes[0] = (long)d_buf.buf_paddr;
d_surface.planes[1] = (long)d_buf.buf_paddr + dst->width() * dst->height();
d_surface.left = 0;
d_surface.top = 0;
d_surface.right = dst->width();
d_surface.bottom = dst->height();
d_surface.stride = dst->width();
d_surface.width = dst->width();
d_surface.height = dst->height();
d_surface.rot = G2D_ROTATION_0;

ret = mBlitEngine(g2dHandle, (void*)&s_surface, (void*)&d_surface);
if (ret == 0) {
mFinishEngine(g2dHandle);
}

0 项奖励
回复

2,326 次查看
joanxie
NXP TechSupport
NXP TechSupport

confirmed that imx8mm doesn't support this, only imx8qxp and imx8qm support this format

0 项奖励
回复

2,670 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the gpu api, gpu should support this format, but what's your case? did you capture video as rgb888 from camera?

0 项奖励
回复