Does freescale provide linux driver demo for imx6ul

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does freescale provide linux driver demo for imx6ul

1,249件の閲覧回数
tony-tony
Contributor III

Hi:

   I wanna know if freescale provide linux driver demo for imx6ul, like how to configure the GPIO reg or other regs.   I want to configure them in my own *.ko file.but don't know if there some demo code I can refer to .

ラベル(1)
0 件の賞賛
返信
1 返信

1,172件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tony

one can look at

Simple GPIO Example - quandry | NXP Community 

and please check i.MX 6UltraLite Linux Binary Demo Files

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_iMX6UL7D&appType=license&location=null&Pare... 

and documentation

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信