Does boot ROM run when Watchdog reset asserted in i.MX7S?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does boot ROM run when Watchdog reset asserted in i.MX7S?

Jump to solution
1,895 Views
T-Ii
Contributor III

Hi, all.

I want to know whether boot ROM run or not when watchdog reset asserted.

 

My customer's product sometimes not wake up from Low Power mode.

I want to find it comes from errata e10574 or not.

 

Thanks.

0 Kudos
Reply
1 Solution
1,823 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
5 Replies
1,887 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using?

0 Kudos
Reply
1,870 Views
T-Ii
Contributor III

Customer doesn't use BSP based OS but proprietary RTOS.

Which point does BPS version affect to watchdog reset?

0 Kudos
Reply
1,861 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

ROM code will start immediately after POR_B deactivated.

2023112.PNG

0 Kudos
Reply
1,844 Views
T-Ii
Contributor III

Thank you for replying.

Let me confirm my understand.

A. boot ROM does not run when watchdog asserted without WDT bit set. (see Figure 6-16. below)

B. boot ROM run when watchdog asserted with WDT bit set. (see Figure 6.17. below)

C. errata e10574 happens in either case.

TIi_0-1673588105748.png

Is my understanding right?

 

Thanks

1,824 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes

0 Kudos
Reply