Does boot ROM run when Watchdog reset asserted in i.MX7S?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does boot ROM run when Watchdog reset asserted in i.MX7S?

ソリューションへジャンプ
1,743件の閲覧回数
T-Ii
Contributor III

Hi, all.

I want to know whether boot ROM run or not when watchdog reset asserted.

 

My customer's product sometimes not wake up from Low Power mode.

I want to find it comes from errata e10574 or not.

 

Thanks.

0 件の賞賛
返信
1 解決策
1,671件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
5 返答(返信)
1,735件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using?

0 件の賞賛
返信
1,718件の閲覧回数
T-Ii
Contributor III

Customer doesn't use BSP based OS but proprietary RTOS.

Which point does BPS version affect to watchdog reset?

0 件の賞賛
返信
1,709件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

ROM code will start immediately after POR_B deactivated.

2023112.PNG

0 件の賞賛
返信
1,692件の閲覧回数
T-Ii
Contributor III

Thank you for replying.

Let me confirm my understand.

A. boot ROM does not run when watchdog asserted without WDT bit set. (see Figure 6-16. below)

B. boot ROM run when watchdog asserted with WDT bit set. (see Figure 6.17. below)

C. errata e10574 happens in either case.

TIi_0-1673588105748.png

Is my understanding right?

 

Thanks

1,672件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes

0 件の賞賛
返信