Hi,
As per below document,
iMX8QXP: Use RPMSG to wake up M4 and A35
patch : L4.14.78_rpmsg_wakeup.patch is for only L4.14.78.
Is there any patch for L4.14.15 as I see there are many changes in rpmsg kernel changes and it looks like not easy to port L4.14.78 patch to L4.1.15?
解決済! 解決策の投稿を見る。
Hi Rakesh
I am afraid such patch is not available for L4.1.15, also it is very old kernel
version no more supported.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Rakesh
I am afraid such patch is not available for L4.1.15, also it is very old kernel
version no more supported.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
In kernel 4.1.15, rpmsg wakeup is default enabled. So it required no patch.
Thanks for your support.
Hi Rakesh Patel
Will you please tell me how you done RPMSG wakeup.
Regards,
Vinoth S,
RPMSG is default wakeup source. You don't require any changes.vinothkumars
Hi rakesh.patel@volansystech.com
I am using latest kernel L4.14.98
Will you please give the patch for Rpmsg or will you please tell me how you done Rpmsg wakeup
Thanks,
Vinoth S,