Does anybody know about a 7'' screen that is compatible with i.MX 6 procesors?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does anybody know about a 7'' screen that is compatible with i.MX 6 procesors?

1,676 Views
trendantenna
Contributor III

I want to stream video into a screen using an i.MX 6

Labels (4)
5 Replies

941 Views
trendantenna
Contributor III

How do I interface the LCD screen F07A-0102 from future electronics? because connect the adapter and then the screen and it only turns the backlight on. I can see that my image boots, through minicom but it isn't displayed on the LCD screen.

0 Kudos

941 Views
OtavioSalvador
Senior Contributor II

I sent the patches for U-Boot which add the proper support for it for merging; I also merged them in

Freescale/u-boot-imx · GitHub

0 Kudos

941 Views
trendantenna
Contributor III

I think I´ve modified the bootloader to support the LCD screen but it onluy turns on it doesn´t display anything. Do I need to make my yocto image support it by modifying the kernel parameters?

0 Kudos

941 Views
OtavioSalvador
Senior Contributor II

The patches are merged in master so it should work.

0 Kudos